Loading
Press Release | January 07, 2021
Recent ActivityRecent Activity

New Inverter Enhances QuickStick HT Intelligent Conveyor System Performance

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

The QuickStick HT intelligent conveyor system from Rockwell Automation is designed to transport large loads with the intelligence of independent cart technology. The most common applications for the technology are in the automotive industry. However, it is also well-suited for heavy-load material handling, ride conveyance and hazardous material handling, including glovebox applications.

The industry-leading system has a new QuickStick HT 5700 inverter, which increases performance. It can now achieve velocities of 5+ m/s. Additionally, the update allows for the use of a smaller Kinetix 5700 power supply, reducing the control cabinet size and saving space on the plant floor. The updated system also includes integrated functional safety. It has hardwired Safe Torque Off and Safe Stop 1 timed, SIL3/PLe.


Click to download image.


Kinetix and QuickStick HT are trademarks of Rockwell Automation Inc.

Published January 7, 2021


  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right