Add an EDD file for a generic HART device

  1. From the Module Properties dialog - General view, select Change...
  2. From the Module Definition dialog, enter the correct Expanded Device Type ID for the HART device, then select Add HART EDD...
    IMPORTANT: The Expanded Device Type ID must match your device. If not, you are not ale to add an EDD file properly.
  3. In the Add HART EDD dialog box, browse to the location of the EDD file.
  4. Select the HART EDD file and select Open.
    The message Successfully added EDD appears.
  5. Select OK to close the dialog box.
    TIP:
    When configuring a device, an error message appears when:
    • The selected file is not an EDD file.
    • An EDD file for the device is not included.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal