HART Device Applications
This chapter describes how to add and monitor HART devices that are connected to your
HART input or output module in a Studio 5000 Logix Designer application project.
You must complete the following tasks before you can configure connection for the HART
device:
- Create a Studio 5000 Logix Designer application project.
- Add a controller to the project.
- Add and configure an analog HART I/O module.
Before using the HART capabilities, verify the following:
- The I/O module and the associated field device are working properly in the analog 4…20 mA mode.
- The channel is configured as 4…20 mA range with HART enabled.
- The field device is HART capable.
- No more than one HART field device is connected to each channel.
- Notch Filter of input channel or Ramping Rate of output channel is set to a valid value.
Input data of HART device that is device status, dynamic, or device variable values and
status, are sent to Logix 5000 controller at the RPI. At the RPI, not only does the
module send input data of the HART devices to the controller, but also the controller
sends data for the HART devices to the module. For example, the controller sends data to
reset Configuration Changed status or initiate an execution of a pre-configured HART
command.
IMPORTANT:
If you switch the controller to Program mode or inhibit an output module, it may
cause the output channels to de-energize and the HART device to not power
up.
To power up the HART device, switch the controller to Run mode and uninhibit the
output module.
Provide Feedback