Controller and Software Compatibility

Controller and programming software compatibility requirements apply when you use PointMax I/O modules. A module type and how it is used affect which requirements apply.
You must use Studio 5000 Logix Designer application version 36 or later. For more information, see the Product Compatibility and Download Center at rok.auto/pcdc.
If you use GuardLogix® controllers and need to use up to chassis slot 32, you must use Studio 5000 Logix Designer application version 37 or later.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal