PointMax I/O in a Logix 5000 Control System
IMPORTANT:
Throughout this publication, the term Logix 5000 controller refers to the
controllers with which you can use PointMax I/O modules in a given capacity.
You can use PointMax I/O modules as the local or remote I/O for CompactLogix
5390* controller, and the remote I/O for CompactLogix 5380, CompactLogix 5480,
ControlLogix 5590, and ControlLogix 5580 controllers, using Studio 5000 Logix
Designer® application version 36 or later (*requires version 39 or later).
You cannot use PointMax I/O modules with all Logix 5000 controllers. For example,
you can use PointMax I/O modules with CompactLogix 5380 and ControlLogix 5580
controllers but not with CompactLogix 5370 and ControlLogix 5570
controllers.
Logix 5000 controllers use I/O modules to control devices in a control system. The
controllers access the modules over an EtherNet/IP network.
See Connections for the communication
model between controller and I/O modules.
Provide Feedback