Use Generic IO-Link Device Profile
With the generic IO-Link device profile, you can add an IO-Link device without a unique
identity.
When you use the generic IO-Link device profile, there is no full IO-Link integration.
You have to configure the device either with an external method or send messages to the
IO-Link Service Parameter object. The process data is presented in raw IO-Link data
format.
To use the generic IO-Link device profile, see Add a Generic IO-Link Device.
Provide Feedback