IO-Link Device Identity
With the highly integrated IO-Link device feature, every IO-Link device has its own
independent CIP identity.
The IO-Link device properties that uniquely identify the type of device are:
- IO-Link Vendor ID
- IO-Link Device ID
- IO-Link Revision
Provide Feedback