IO-Link Device Electronic Keying
The Electronic Keying feature for IO-Link devices automatically compares the expected
device to the physical device before connection is established. You can use Electronic
Keying to help prevent connection to a device that does not match the type and revision
expected.
For each device, the selected keying option determines if, and how, an Electronic Keying
check is performed.
The three keying options that are available are:
- Compatible Module (default)
- Exact Match
- Disable Keying
Compatible Module is the default setting. The following three keying attributes of the
configured device and the physical device must match:
- IO-Link Vendor ID
- IO-Link Device ID
- IO-Link Revision
If the Exact Match option is selected, the following four keying attributes of the
configured device and the physical device must match:
- IO-Link Vendor ID
- IO-Link Device ID
- IO-Link Revision
- Device Firmware Revision
Also for Exact Match, the physical device must not be emulating another device (if the
device supports multiple device IDs).
Disable Keying indicates that the keying attributes are not considered when attempting to
communicate with a IO-Link device. With Disabled Keying, the IO-Link connection can
occur with a device other than the type specified in the I/O configuration tree with
unpredictable results.
WARNING:
Be extremely cautious when using Disable Keying; if used incorrectly, this option
can lead to personal injury or death, property damage, or economic loss.
You do not use Disable Keying. If you use Disable Keying, you must take full
responsibility for understanding whether the device being used can fulfill the
functional requirements of the application.
Provide Feedback