Replace a Master Module and Devices with Device ADC Disabled
Verify that you have completed the procedure as described in Prerequisite Steps.
To replace an IO-Link master module and all IO-Link devices in this scenario, complete
these steps.
- In the IO-Link master Module Properties → Connection view, select the Inhibit Module checkbox and select Apply.
- Replace the IO-Link master module and IO-Link devices.
- In the IO-Link device Module Properties → Configuration view, perform Device Correlation Check and select “Use Project Values”.Repeat this step for all IO-Link devices with ADC disabled.
- In the IO-Link master Module Properties → Connection view, clear the Inhibit Module checkbox and select Apply.
Provide Feedback