Replace a Device on a Fallback Channel
WARNING:
Before you replace a device that is assigned to a
Fallback channel, you must first inhibit the device. To replace a device on a Fallback
channel, complete these steps.
- Go online with your project.
- In the IO-Link device Module Properties → Connection view, select the Inhibit Module checkbox and select Apply.
- Follow the steps that are described in the other scenarios that apply to your device.
- After you have completed those steps, in the IO-Link device Module Properties → Connection view, clear the Inhibit Module checkbox and select Apply.
Provide Feedback