Muting Lamp Operation
To use test outputs for muting lamp operation, select Muting Lamp for the Test Output
Point Mode in the Module Properties dialog.
Your controller program controls test outputs 0…3 (TO0…TO3) to illuminate a muting lamp.
Muting lamp status is monitored with a test that runs periodically during every test
interval to detect a burned-out lamp. The test runs repeatedly when the test output is
commanded On or commanded Off and a fault is detected.
Monitor Muting Lamp Operation, Status, and Fault Detection
TIP:
The lamp test interval is 2 seconds. Two consecutive failed lamp tests are
required to declare a burned-out lamp condition.
The lamp test does not always run immediately after the test output is energized.
It starts at the next 2-second interval. To allow time for two consecutive test
intervals, program a minimum Test Output On Time of 4 seconds.
Test Output Commanded State | Lamp Condition | Muting Status Bit | Required Action |
|---|---|---|---|
ON | Bad (open circuit) | 0 | Repair the lamp. |
ON | Good | 1 | None, normal condition, the lamp is operating properly. |
OFF | Bad (open circuit) | 0 | If the lamp remains OFF after the test output is cycled, repair
the lamp. |
OFF | Good | 1 | None, normal condition |
| |||
Provide Feedback