Terminology
This table defines the terms that are used in this publication.
Acronym | Full Term | Definition |
|---|---|---|
BOOTP | Bootstrap Protocol | A computer networking protocol used to automatically assign an IP address to
network devices from a configuration server. |
BP | Backplane Power | Power that is generated from module power by the adapter and expansion power, and
supplied to the I/O system through the backplane. |
CIP™ | Common Industrial Protocol | An industrial communication protocol that is used by Logix 5000® based automation
systems on EtherNet/IP™, ControlNet®, and DeviceNet® communication networks. |
CIP Sync™ | Common Industrial Protocol Synchronization | CIP Sync provides the increased control coordination needed for control
applications where absolute time synchronization is vital to achieve real-time
synchronization between distributed intelligent devices and systems. |
DHCP | Dynamic Host Configuration Protocol | A network protocol used to automate the process of assigning IP addresses and
other network configuration parameters to devices on a network. |
DLR | Device Level Ring | A network technology that takes advantage of embedded-switch functionality in
automation devices. |
MB | Mounting Base | A device that provides data and power connections from the backplane to the
installed module. |
MP | Module Power | Power that is supplied to the adapter and expansion power. |
NFC | Near Field Communication | A short-range wireless technology that enables communication between two
electronic devices over a distance of 4 cm (1.6 in.) or less. |
ODVA | Open DeviceNet Vendor Association | A nonprofit association of vendors that are established for the promotion of CIP
networks. |
PRP | Parallel Redundancy Protocol | An EtherNet /IP specification used to create network redundancy by allowing PRP
enabled devices to send duplicate Ethernet frames over two independent Local Area
Networks (LANs). |
RIUP | Removal and Insertion Under Power | A feature that enables the device to be connected and disconnected from the
system without having to remove power from the system. |
RPI | Requested Packet Interval | Time interval (usually in milliseconds) that users are requesting their data be
exchanged at |
RTB | Removable Terminal Block | A component that is used for wiring field devices to. |
SA | Sensor Actuator - Power | Sensor Actuator Power (24V DC nominal) for the field devices. |
SELV | Safety Extra Low Voltage | An electrical system where the voltage level is considered safe under normal or
fault conditions, as defined in the EN and IEC standards. |
XT | Extreme Environment | Modules with XT at the end of their catalog numbers have design considerations
and conformal coating that add a degree of protection for harsh, corrosive gas
environments. |
Provide Feedback