Select the Network Redundancy Mode

The PointMax EtherNet/IP adapter supports two types of network redundancy:
  • DLR (Device Level Ring)
  • PRP (Parallel Redundancy Protocol)
In these modes, all EtherNet/IP ports of the adapter are used to provide redundant network paths.
IMPORTANT:
Make sure that both EtherNet/IP ports are enabled and configured correctly (recommended setting: auto-negotiation is ON).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal