Set the Network Address with Rotary Switches

To adjust the network address switches, do the following:
  1. Remove power from the adapter.
  2. Lift the IP switch cover using the tab marked with the symbol to open it. For instructions on removing and replacing the network address cover, see Remove and Replace the Adapter Network Address Door
  3. Set the network address to a valid value.
    Use a small flat screwdriver or test pen to rotate each network address switch and align the arrow with the desired number (0…9).
  4. Lower the IP switch cover and press it down until it clicks into place to close it.
  5. Reapply power to the adapter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal