Axis Properties - Autotune Dialog Box Overview (AXIS_CIP_DRIVE)

Use the
Autotune
page to perform an autotune to improve the performance of the system.
TIP:
Autotune
category is available only when
Axis Configuration
on the
General
page is set to
Position Loop
or
Velocity Loop
.
TIP: To open the Autotune page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    Autotune
    .
This table describes the settings on the page:
Parameter
Description
Application Type
Used to select the type of application to be tuned.
The available values include:
  • Basic
  • Tracking
  • Point to Point
  • Constant Speed
  • Custom
The default value is
Basic
.
TIP: Changing the Application Type value affects other attributes (Velocity Integrator Hold, Position Integrator Hold, Gain Tuning Configuration Bits).
Application Type
is unavailable when the axis is Servo On.
Loop Response
Used to select how tightly or hot the system tunes.
The available values include:
  • Low
  • Medium
  • High
The default value is the current value of the attribute.
TIP: Changing the Loop Response value affects the Damping Factor attribute.
Loop Response
is unavailable in online mode and when the axis is Servo On.
Load Coupling
Used to select how tightly the system is physically coupled.
The available values include:
  • Rigid
  • Compliant
The default value is the current value of the attribute.
Applying changes to the Coupling value causes changes to the gain values that are displayed in the Gains Tuned grid in the right panel of the
Autotune
tab.
Load Coupling
is unavailable in online mode and when the axis is Servo On.
Position Integrator Bandwidth
Used to calculate the position integrator bandwidth.
The position integrator bandwidth only applies when the Axis Configuration on the
General
tab is set to
Position Loop
. When the Axis Configuration is not set to
Position Loop
, this control is unavailable and you cannot modify it.
When
Application Type
is set to
Custom
and the application is in offline mode, this check box is enabled and you can modify the setting.
Position Integrator Bandwidth
is unavailable:
  • In online mode when the axis is Servo On.
  • When the Application Type is not set to Custom.
Velocity Integrator Bandwidth
Used to calculate the
Velocity Integrator Bandwidth
.
When Application Type is set to
Custom
, this check box is enabled, and you can modify the setting.
Velocity Integrator Bandwidth
is unavailable:
  • In online mode when the axis is Servo On.
  • When the Application Type is not set to Custom.
Velocity Feedforward
Used to calculate the
Velocity Feedforward
.
The
Velocity Feedforward
only applies when the Axis Configuration on the
General
tab is set to
Position Loop
. When the
Axis Configuration
is not set to
Position Loop
, this control is unavailable and you cannot modify it.
When
Application Type
is set to
Custom
, this check box is enabled. and you can modify it.
Velocity Feedback
is unavailable:
  • In online mode when the axis is Servo On.
  • When the
    Application Type
    is not set to
    Custom
    .
Acceleration Feedforward
Used to calculate the
Acceleration Feedforward
.
When
Application Type
is set to
Custom
, this check box is enabled. and you can modify the setting.
Acceleration Feedback
is unavailable:
  • In online mode when the axis is Servo On.
  • When the Application Type is not set to Custom.
Torque Low Pass Filter
Used to calculate the
Torque Low Pass Filter
.
When
Application Type
is set to
Custom
, this check box is enabled, and you can modify the setting.
Torque Low Pass Filter
is unavailable:
  • In online mode when the axis is Servo On.
  • When the Application Type is not set to Custom.
Measure Inertia using Tune Profile
Used to calculate the Inertia Tuned values as part of the Autotune.
The Inertia Test results are shown in the Inertia Tuned grid control (bottom right of this tab) when the test completes.
Measure Inertia
is unavailable in offline mode as well as in online mode when the axis is Servo On.
Motion with Load
Used to calculate information based on the load inertia.
The load inertia is measured and applied to the
Total Inertia
attribute or
Total Mass
attribute. If the value for
Rotary Motor Inertia
or
Linear Motor Mass
is non-zero, the Load Ratio is also updated.
Total Inertia
and
Rotary Motor Inertia
apply to rotary motors. Total Mass and Linear Motor Mass apply to linear motors.
The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection.
Motion with Load is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Uncoupled Motor
Used to calculate information based on the motor inertia.
If selected, when the test is run, the motor inertia is measured and is stored in the
Rotary Motor Inertia
attribute or
Linear Motor Mass
attribute.
Rotary Motor
Inertia applies to rotary motors.
Linear Motor Mass
applies to linear motors.
The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection.
Uncoupled Motor
is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Travel Limit
Used to specify the maximum distance to travel for the tune operation.
The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection.
Travel Limit
is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Speed
Used to specify the speed of the tune operation.
The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection.
Speed
is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Torque
Used to enter a value that specifies the torque value that is to be applied to the tune operation. The default value is 100.
The blue arrow next to a control indicates that the data is immediately committed. You cannot undo the selection.
Torque
is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Direction
Used select the direction of the move for the tune operation.
The available values include:
  • Forward Unidirectional
  • Reverse Unidirectional
  • Forward Bi-Directional
  • Reverse Bi-Directional
The default value is
Forward Unidirectional
.
The blue arrow next to a control indicates that the data is immediately committed. You do not have the opportunity to undo the selection.
Direction
is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • Inertia Tune is false.
Start
Used to initiate an autotune operation.
When the Measure Inertia check box is selected, a request is issued to the controller to start a tune.
Pending edits need to be applied before you start the test. If you have pending edits, a dialog box opens informing you that pending edits will be applied prior to executing the test. You can choose Yes or No to apply the pending edits. If you choose No, the test will not be executed.
Clicking the Start button issues a Motion Direct Command to the controller, which causes any parameters used by the Motion Direct Command to validate before starting the test.
If the Motion Direct Command does not execute due to an error condition, an error message displays and the Test State returns to the Ready state
Start is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • When a tune is in progress.
Stop
Used to terminate an autotune operation that was started somewhere other than the Autotune dialog box that is displayed.
When an Autotune is started from the
Start
button on this dialog box, this Stop button is not available.
This
Stop
button is only available if the Autotune was started from the user program Motion Run Axis Tuning (MRAT) or when multiple workstations are used and the Autotune is started from a different workstation.
The stop tune issues a Motion Direct Command to the controller.
Stop is unavailable:
  • In offline mode.
  • In online mode when the axis is Servo On.
  • The tune is ready to be executed.
Danger
Used to displays warning information about the tuning operation.
Danger text is unavailable in offline mode and when the Measure Inertia check box is not selected.
Tune Status
Used to display the status of the tuning operation.
Tune Status values include:
  • Ready
  • Success
  • Executing
  • Stopped by User
  • Time-Out Fault
  • Servo Fault
  • Exceeded Travel Limit
  • Axis Polarity Set Incorrectly
  • Measurement Fault
  • Configuration Fault
The default value is Ready.
Loop Parameters Tuned
Contains one column that lists the current attributes and one column that lists the calculated results of the tuning operation.
Rows Header
Contains a splat (*) when the Tuned Value is not the same as the Current Value.
Name
Displays the name of the attribute.
Current Value
Displays the value of the gain attribute from the controller.
Tuned Value
Contains the tuned value for the attribute.
Tuned Values may be calculated by the autotune. When a gain is no longer used in the tune calculation (the corresponding check box in the Customize Gains to Tune group is not selected), the Tuned Value is set to zero. The tuned value column becomes blank until a tune operation is started. Once started, the data updates, regardless of the completion status.
Unit
Contains the units that are associated with the corresponding attribute.
TIP: Attributes that do not apply to the current configuration are not shown in the grid.
Advanced Compensation
Used to expand and the minus sign to collapse the
Advanced Compensation
section.
The default is that the
Advanced Compensation
section is collapsed.
The
Advanced Compensation
section is unavailable in offline mode as well as in online mode when the axis is Servo On.
Inertia
Used to enter an inertia value to be used in tuning calculations.
If the
Use Load Ratio
check box is selected on the Load dialog box, this attribute is a measure of load ratio. Otherwise, this attribute is a measure of tune inertia mass.
Inertia is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
Compensate check box for Inertia
Used to calculate the inertia value in the tuning procedure.
The Compensate check box for Inertia is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
  • When this check box is cleared.
If you run the tune operation with Measure Inertia selected, the controller returns the inertia value. If Inertia is checked, the value is used in the tune equations. You can enter a different inertia value, then re-run the tune calculations using the specified value.
Friction
Used to enter a friction value in tuning calculations. Friction is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
Compensate check box for Friction
Used to calculate the Friction value in the tuning procedure.
The Compensate check box for Friction is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
  • When this check box is cleared.
If you run the tune operation with Measure Inertia checked, the controller returns the friction value. You can enter a different friction value, then re-run the tune calculations using the specified value.
Active Torque
Used to enter an active torque value in tuning calculations.
Active Torque
is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
Compensate check box for Active Torque
Used to calculate the active torque value in the tuning procedure.
The Compensate checkbox for
Active Torque
is unavailable:
  • In offline mode.
  • When the axis is Servo On.
  • When Inertia Tune is not selected.
  • When the Tune Status is Success.
  • When this check box is cleared.
If you run the tune operation with Measure Inertia selected, the controller returns the active torque value. You can enter a different active torque value, then re-run the tune calculations using the specified value.
Calculate Compensation
Used to calculate the compensation values.
Calculate Compensation
is unavailable in offline mode.
Load Parameters Tuned
Contains one column that lists the current attributes and one column that lists the calculated results of the tuning operation.
Rows Header
Contains an asterisk (*) when the Tuned Value is not the same as the Current Value.
Name
Used to displays the name of the attribute.
Current Value
Used to displays the value of the gain attribute from the controller.
Tuned Value
Contains the tuned value for the attribute. One column lists the current attributes and one column lists the calculated results of the tuning operation.
Tuned Values may be calculated by the autotune. When a gain is no longer used in the tune calculation (that is, the corresponding check box in the Customize Gains to Tune group is not selected ), the Tuned Value is set to zero. The tuned value column becomes blank until a tune operation is started. Once started, the data updates, regardless of the completion status.
Unit
Contains the units that are associated with the corresponding attribute.
TIP: Attributes that do not apply to the current configuration are not shown in the grid.
Accept Tuned Values
Used to commit the values from the Tuned Value columns of the grid to the attribute, causing the Current Value column to update.
The blue arrow next to a control indicates that the data is immediately committed. You do not have the opportunity to undo the change.
The
Accept Tuned Values
button is unavailable in offline mode and if no test was successfully completed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal