View task performance details

Use the
Monitor
tab of the
Task Properties
dialog box to view specific details of task operations.
From this tab, view information on scan times, the elapsed interval time between triggers, and the number of task overlaps.
TIP:
Overlaps do not occur for Safety tasks, since the Watchdog value must always be less than or equal to the task period.
Selecting the
Reset
button resets the values displayed on the tab.
TIP: To open the Monitor tab on the Task Properties dialog:
  • From the
    Edit
    menu, select
    Properties
    .
  • From the Controller Organizer, right-click the
    Task
    folder and select
    Properties
    .
    The
    Task Properties
    dialog is displayed, with the
    General
    tab selected. Select the
    Monitor
    tab to view the information available there.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal