Edit a task configuration

Use the
Configuration
tab of the
Task Properties
dialog box to edit task configuration parameters once the task is created.
To edit a task configuration:
  1. Open the
    Configuration
    tab of the
    Task Properties
    dialog box:
    • From the
      Edit
      menu, choose
      Properties
      .
    • From the Controller Organizer right-click the
      Task
      folder and choose
      Properties
      from the menu.
      The
      Task Properties
      dialog box appears, with the
      General
      tab selected. Click the
      Configuration
      tab to configure the selected task.
  2. Follow the steps that correspond to the task type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal