Define the steps of an SFC process
A step represents a major function of the process.
A step contains the actions that occur at a particular time, phase, or station.

![]() | step |
![]() | transition |
| |
A transition ends a step. The transition defines the physical conditions that must occur or change in order to go to the next step.
Provide Feedback