Plug-In Manager dialog box parameters
The
Plug-In Manager
dialog box includes the following parameters.Item | Description |
Plug-Ins | A list of Logix Designer application plug-ins. Plug-ins appear in this list if a plug-in is registered for the current version of Logix Designer application or if custom properties exist in the project. |
Description | Plug-in descriptions. When you select a plug-in, its description appears here. The Description field is blank for plug-ins that are not registered. |
Version | The current version of the selected plug-in. |
Status | Indicates whether the selected plug-in is registered or not registered with Logix Designer application. Also indicates failed registrations for plug-ins with invalid configurations. |
Has Custom Properties | Indicates whether properties exist for the selected plug-in.
|
Remove All Custom Properties for Plug-In | Click this option to remove all the custom properties in the current project associated with the selected plug-in. This option is not available if there are no custom properties for the plug-in. |
Provide Feedback