Accept modifications
Any action performed while editing a Ladder element’s field accepts the current edit.
Press Enter to accept an edit of a ladder element field. This accepts the edit and moves the caret to the next operand field/download value field (whichever comes first) of the same instruction. If the caret is at the last operand of the instruction, the caret does not move and editing stops.
Press Tab to accept an edit of an instruction field. This accepts the edit and moves the caret. If the edit is not being done on an instruction, the caret is not moved.
Left-click to accept the edit. This accepts the edit and performs the action.
Provide Feedback