Feedback configurations
Choosing a data source other than
Nameplate Datasheet
on the Motor
page and the selection of the Feedback Configuration
on the General
page, determine which Feedback pages display in Axis Properties
dialog box:If Feedback Configuration on the General page is set to: | This page displays: |
Master Feedback | Master Feedback |
Motor Feedback | Motor Feedback |
Load Feedback | Motor Feedback and Load Feedback |
Dual Feedback/Dual Integral Feedback | Motor Feedback and Load Feedback |
TIP:
If
Data Source
on the Motor
page is set to anything other than Nameplate Datasheet
, the motor provides the information displayed on this page.The controls on this page are unavailable when online with the controller.
Provide Feedback