Create a motion group
Create a motion group if one does not already exist, and associate an axis to the group. Then add the axes to the project's motion group.
To create a motion group and associate an axis to the motion group:
- Right-click the axis, and selectProperties. TheAxis Propertiesdialog box appears.
- InCategories, selectGeneral.
- In theAssigned Grouparea, clickNew Group.
- In theName, type a tag name.
- (optional) In theDescription, type a description of the tag.
- InData Type, selectMOTION_GROUP.
- InScope, select the scope.
- InExternal Accesslist, select the external access type.
- InOPC UA Access, select the OPC UA access type.
- Select theOpen MOTION_GROUPcheck box, and selectCreate. TheMotion Group Wizarddialog box appears.
- In theUnassignedpane, select the axis to associate to the group and selectAdd.
- (optional) SelectNextto configure the base update period.
- SelectFinish.
Provide Feedback