Coordinate System Properties - Offsets
Use the settings on the
Offsets
tab in the Coordinate System Properties
dialog box to define the end effector and base offset values for the robotic arm. The
Offset
tab shows the views of a typical robotic arm based on the configuration of the robot geometry type on the General
tab. The type of offsets and the number of available offsets is determined by the coordinate system and the number of axes associated with the coordinate system.When specifying the end effector and base offset values, be sure that the values are calculated using the same measurement units as the linked Cartesian coordinate system. For example, if the manufacturer specifies the robot offset using millimeter units and you want to configure the robot using inches, then convert the millimeter link measurements to inches and enter the values in the appropriate offset fields.
TIP:
To open the Offsets tab:
- In theController Organizer, expand theMotion Groupfolder, and double-click the coordinate system.
- On theCoordinate System Propertiesdialog box, select theOffsetstab.
Provide Feedback