Coordinate System Properties - Dynamics
Use the settings on the
Dynamics
tab in the Coordinate System Properties
dialog box to enter Vector, Actual and Command Position Tolerance, and Orientation values for a Cartesian coordinate system.The
Dynamics
tab is only available when configuring a Cartesian coordinate system.
TIP:
To open the Dynamics tab:
- In theController Organizer, expand theMotion Groupfolder, and double-click the coordinate system.
- On theCoordinate System Propertiesdialog box, on theGeneraltab, selectCartesianas theType.
- Click theDynamicstab.
Provide Feedback