Calculate Position Parameters Dialog Box Overview (AXIS_SERVO_DRIVE)

Use this dialog to calculate Drive Resolution and Conversion Constant values, based on specific Position Unit Scaling and Position Range information.
  1. In the Position Unit Scaling field, enter the number of position units you want to move for the specified number of motor revolutions.
  2. In the per (Motor Rev) field, enter the number of motor revolutions you want to cover per position unit.
  3. In the Position Range field, enter the number of position units that indicates the distance you want the axis to move.
  4. Click Calculate to calculate the Drive Resolution and Conversion Constant values.
  5. Choose the motor you want and click OK to return to the Axis Properties dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal