Tag-based alarms

Use
Logix Designer
tag-based alarms to monitor a tag value to determine the alarm condition. Tag-based alarms monitor tag values to determine the alarm condition, but they are not part of the logic program and do not increase the scan time for a project.
TIP:
Tag-based alarms are supported only on
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal