Open/Import Project Dialog Box - Source Control View

Use this dialog box to open a project file or to perform a full import of a project file from Source control view.
Parameters
Parameter
Description
Look in:
Select the directory in the AssetCentre archive where the project to open or import resides. (The last open location is remembered upon subsequent returns.)
Up One Level - Up_One_Level
Move up one level in the directory tree.
Active when logged in to a server or database and if not already at the top level of the tree.
View Menu - View_menu
Select the view type (view list of file names or list of file names with username).
Active when logged in to a server or database.
Login - Login
Log in to a specific server and attach to a specific database.
Manage Server Registrations - Manage_Server_Registrations
Open a dialog box to manage one or more server or database combinations.
Select Version or Label for the Operation - select_version_or_label_for_the_operation
Select an archived element based on either version or a label.
Active when file selected.
Search for Files or Folder - search_for_files_or_folders (2)
Select to search for either files or folders within the current archive database.
Active when logged in to a server or database.
Help - Help
View source control help.
Directory/File
Displays directories and files contained within a specific server or database. The View Menu determines the view type (either list or details).
Check Out
If unselected, retrieves a copy of the selected file when selecting Get.
If selected, the file to retrieve is checked out.
Not selected and not active if selected file is already checked out.
File Name
Displays the currently selected file (read-only).
Files of type:
Choose the type of file to open or import (ACD file is the only option).
Get
Retrieve (get) the file or check out the file (if Check Out box is selected).
Active if logged in to a server or database and if a file is selected to retrieve.
Cancel
Cancel the open or import and close the Open/Import Project dialog box.
Help
View help about Open/Import Project dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal