Error creating task
The error message indicates a condition that prevents the creation of the task:
Name is invalid
Entered an invalid name. Re-enter a valid name.
Watchdog is invalid
.Entered a Watchdog that is outside the valid range. Re-enter the Watchdog.
Priority is invalid
Entered a Priority that is outside the valid range. Re-enter the Priority.
Rate is invalid
Entered a Rate that is outside the valid range. Re-enter the Rate.
Event Task Conditions
Specify a valid EventTag to set the EventTrigger for this task.
- Correct the Invalid Trigger and Tag combination.
- The Tag and Trigger combination is already in use in another Event Task.
- The selected Input Module is not capable of triggering and event.
- The Axis Tag used in this Event Task does not have the capability to trigger an event.
- The tag used for the event task does not exist.
Provide Feedback