Create a DataStore with sample data types

Create a DataStore with sample data types

Create a database with sample data types to populate and export to a
CSV
file.
  1. Create an Embedded database. See Create a database.
  2. Hover-over the database, select
    Edit
    , and enter
    Store1
    .
  3. Configure the following table columns:
    Column number
    Data type
    1
    Int16
    2
    Int32
    3
    Float
    4
    String
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal