Copy a Program Organization Unit from one session and paste it to another

Open multiple sessions of
FactoryTalk Design Workbench
, and then copy Program Organization Units (POU) from one open session to another open session. The copied POUs reserve their configuration options.
To copy a POU from one session and paste it to another
  1. Open a session of
    FactoryTalk Design Workbench
    , and then create a project or open an existing project.
  2. Open another session and another project.
  3. In one session, right-click the POU, and then select
    Copy
    .
  4. In another session, in
    Project Organizer
    , double-click the node under which you want to paste the POU, and then select
    Paste
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal