Import a project
Use the
Welcome
page or the File
menu to import a project to FactoryTalk Design Workbench
.- You cannot import a project created in a later version ofFactoryTalk Design Workbenchto an earlier version.
- You can import a project with the following controller types fromConnected Components Workbenchversion 22.00 or 23.00 toFactoryTalk Design Workbench:Controllers supporting legacy project importController TypeSupported RevisionMicro810R7.00L20ER23.00L50ER22.00 or laterL70ER22.00 or later
- You cannot import a project created inFactoryTalk Design WorkbenchtoConnected Components Workbench.
- The import file format is CCWARC forConnected Components Workbenchprojects or FTDWA forFactoryTalk Design Workbenchprojects.
Prerequisites
- Close any open project.
- The controller is offline.
To import a project
- OpenImport projectby doing one of the following:
- From theWelcomepage, selectImport project.
- From theFilemenu, selectImport project.
- InImport project, selectBrowse.
- InOpen, locate and select the file, and then selectOpen.
- InImport project, selectImport.Duplicated project names are appended with a number to avoid overwriting the existing project files.
Provide Feedback