Verify a Program Organization Unit
Use the
Verify program
context menu to verify the logic of a single Program Organization Unit (POU) without building the whole solution. The verification result shows on the Output
pane. On Project Organizer
, a symbol will display next to the POU name to indicate any errors or warnings.To verify a POU
- InProject Organizer, right-click the POU, and then selectVerify program.
Provide Feedback