Rename a user-defined function
Use
Project Organizer
to rename a user-defined function (UDF). Renaming a UDF automatically updates all references to the UDF.To rename a UDF
- InProject Organizer, go to .
- ExpandUser-Defined Functions, and then do one of the following:
- Select the UDF you want to rename.
- Right-click the UDF you want to rename, and then selectRename.
- In theUser-defined functionbox of thePropertiespane, enter the new name.
Provide Feedback