Add a user-defined function block using Project Organizer
Use
Project Organizer
to add a user-defined function block to the controller project.To add a user-defined function block using Project Organizer
- InProject Organizer, right-clickUser-Defined Function Blocks, and then selectNew user-defined function block.
- InNew user-defined function block, enter the UDFB name, select the UDFB type, and then enter the description as needed.
- SelectCreate.
Provide Feedback