Add Program Organization Unit descriptions
Use the
Description
box in the Properties
pane to document individual Program Organization Units (POUs). For example, you can document the implementation details of a POU.Descriptions are automatically saved and stored in rich text format (*.rtf).
To add POU descriptions
- InProject Organizer, select the POU.
- In thePropertiespane, in theDescriptionbox, enter the description.
Provide Feedback