Structured text basic elements and statements

Structured text (ST) elements and statements are the components used to create an ST program.
The following ST elements and statements can be added to your ST program from the ST
Toolbox
in
FactoryTalk Design Workbench
:
The following statements are not available from the ST
Toolbox
. Enter the statements in the ST editor to add the statements:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal