Add a ladder diagram branch

Instructions placed in a branch direct the Program Organization Unit (POU) to use:
  • The instruction in the rung
  • The instruction in a branch
  • The instruction in a branch level
  • The instruction in the next branch level
To add a ladder diagram branch
  • From
    Toolbox
    , drag Add branch button to a valid location.
    green dot indicating a valid location indicates a valid dropping location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal