Search
FactoryTalk Design Workbench Help
Programming languages
Micro800
controllers and
FactoryTalk Design Workbench
support the following programming languages:
Structured text language (ST) elements
Ladder diagram (LD) language elements
Function block diagram (FBD) language elements
Micro800 controller
Compliance with IEC61131-3
Language editors
Ladder diagram language
Function block diagram language
Structured text (ST) language
User-defined function blocks
User-defined functions
Monitoring local variables for user-defined functions and user-defined function blocks
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal