Operators

The
FactoryTalk Design Workbench
instruction set includes IEC 61131-3-compliant instruction blocks for
Micro800
controllers; operators are included in the
Micro800
instruction set.
An operator performs basic logical operations like arithmetic, Boolean logic, comparisons, or data conversions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal