Add a data set descriptor
Use the
DNP3 Data Set Descriptor
configuration page to add, edit, or delete data set descriptors.Prerequisites
- SelectDNP3 slaveas the drive.
To add a data set descriptor
- In theControllertree, expandDNP3 Slave, and then selectDNP3 Data Set Descriptor.
- On theDNP3 Data Set Descriptorpage, selectNew DS.
- UnderDS<x>, selectAdd.xis the index number of the data set you just added.
- (optional) SelectEnable eventto configure event settings.TIP:
- To edit a data set descriptor, select the data set descriptor, and then selectEdit.
- To delete a data set descriptor, select the data set descriptor, and then selectDelete.
Provide Feedback