Function files

Function files do not consume user memory.
Each input or output data element consumes around three user words because of the overhead associated with I/O forcing. Because of the controller's limited user memory, although the controller supports up to 256 elements in a file, creating a file with 256 elements might not be possible.
The
Micro800
controller supports 20 kilobytes of program files and data files in total. The maximum data memory usage is 10,000 words.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal