Back up programs and project files to the memory module
Use the
Back up to the memory module
button on the 2080-MEMBAK-RTC2 plug-in module configuration page to back up user programs and controller project files to the 2080-MEMBAK-RTC2 plug-in module.Prerequisites
- The 2080-MEMBAK-RTC2 plug-in module is detected.
- The controller is inRemote programmode.
To back up programs and project files to the memory module
- InProject Organizer, go to , and then do one of the following:
- Double -click2080-MEMBAK-RTC2.
- Select2080-MEMBAK-RTC2, and then select theEnterkey.
- On the2080-MEMBAK-RTC2page, selectMemory Module.
- On theMemory Moduleconfiguration page, selectBack up to the memory module.
- InMemory module, selectBack up.
- SelectClose.
Provide Feedback