Replace an expansion module
Use these steps to replace an expansion module with another one in a controller project.
Prerequisites
- To replace a module using theReplace modulemenu, at least one module must be added to the controller.
- To replace a module using theNew modulemenu, at least two modules must be added to the controller, and the module you want to replace is not in the last slot.
To replace an expansion module
- Do one of the following:
- To replace an expansion module using theReplace modulemenu
- InProject Organizer, go to .
- ExpandExpansions, right-click the module you want to replace, and then selectReplace module.
- InAdd module, select the new module, and then selectAdd.
- InDevices definition, configure the settings as needed, and then selectOK.
- To replace an expansion module using theNew modulemenu
- InProject Organizer, go to .
- ExpandExpansions, right-click the module you want to replace, and then selectDelete.
- InWarning, selectNO.
- UnderExpansions, right-clickAvailable, and then selectNew module.
- InAdd module, select the new module, and then selectAdd.
- InDevices definition, configure the settings as needed, and then selectOK.
Provide Feedback