Add an Ethernet device

Use
Project Organizer
to add an Ethernet device to a project.
To add an Ethernet device
  1. In
    Project Organizer
    , expand
    I/O Configurations
    .
  2. Right-click
    Ethernet
    , and then select
    New device
    .
  3. In
    Add device
    , select a device, and then select
    Add
    .
  4. In
    Devices definition
    , configure the parameters, and then select
    OK
    .
    A
    <device-name>
    node is created under
    Ethernet
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal