Loading
Press Release
Recent ActivityRecent Activity

Rockwell Automation supports environmentally friendly lithium production to secure UK supply

Modern DCS from Rockwell Automation provides reliable control for Cornish Lithium's demonstration plant.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Mining tentacles in an open pit mine

Rockwell Automation, Inc. (NYSE: ROK), the world's largest company dedicated to industrial automation and digital transformation, is working with Cornish Lithium Plc on a demonstration plant to validate the sustainable production of lithium hydroxide from micaceous granite. According to the International Energy Agency (IEA), the world could face lithium shortages by 2025. To hit net zero targets by 2050, it is estimated that more than 2 billion electric vehicles are needed worldwide, and these vehicles require lithium for their batteries. However, the lithium resources required to meet this surging demand are concentrated in only a few regions around the globe.

The Cornish Lithium demonstration plant will be controlled by the PlantPAx® modern distributed control system from Rockwell Automation. This modern DCS provides a single, plant-wide control system and increased flexibility for better business decisions.

“Rockwell Automation has both the technology and domain expertise to support the complex lithium extraction process,” said Phil Hadfield, UK managing director, Rockwell Automation. “We have successfully worked in lithium projects around the world, including Australia, Africa, and South America. The integrated architecture from Rockwell Automation provides end-to-end system integration. The systems are designed with scalability in mind, leveraging the new advancements in digital technology.”

Cornish Lithium has licensed an acid-leaching, selective precipitation, and crystallization process developed to create lithium hydroxide from micaceous granite. This process is expected to be more environmentally friendly than the traditional hard rock process, which usually involves a significant calcination step, where the ore is calcined at 1,000°C.

The validity of the process has already been tested at a small pilot plant in Australia and proven that it can produce lithium hydroxide monohydrate salt. The next step is constructing a demonstration plant at the site in Cornwall. This will be a complete conceptual end-to-end process from the raw material to lithium hydroxide, using all the same equipment employed in a full-scale facility with just one or two changes for scale reasons. This simulation of the actual process will assure all stakeholders and potential customers of the effectiveness of the processing technology on Cornish ore ahead of the construction of a full-scale production facility.

 "Rockwell Automation will play quite a crucial role in what we are doing," said David Moseley, process manager, hard rock minerals, at Cornish Lithium. "We want to try and simulate as much as possible, the industrial process control that we might employ at full scale. We are trying to put as much of that into the demonstration plant as possible because it is a complex multistage process with lots of recycles - and sequential operation, particularly with filtration, and process control is critical. Rockwell Automation is putting together the process control philosophy based on our instrumentation. This is a series of different process control units that must be coordinated to have a plant that will operate effectively."

Cornwall has a rich mining heritage. A large granite outcrop dominates the geology in the southwest of the UK, and because of millennia of geothermal activity, that granite is rich in lithium. As a result, the concentration of certain minerals, such as tin and copper, has been prevalent. Cornwall is also home to a globally significant china clay industry, and that china clay or Kaolin operation exploits the same granite resource.

Two plants will be built; one is a mineral concentration plant where raw ore is crushed, milled, and separated to create lithium-enriched mica concentrate. The second is the chemical plant, with a hydrometallurgical acid leaching system that produces lithium sulfate, which is converted into lithium hydroxide. The chemical plant combines chemical reactors, precipitators, filtration, and crystallization. The demonstration plant is currently under construction and when commissioned is expected to operate for a year.

 

About Cornish Lithium

Cornish Lithium is a pioneering mineral exploration and development company

focused on the environmentally-sustainable extraction of lithium from geothermal waters and hard rock in the historic mining district of Cornwall. The Company has secured agreements with the owners of mineral rights over a large area of the County and is using modern technology to re-evaluate the region for its potential to produce lithium and other vital technology metals in a low carbon and low impact manner. A secure domestic supply of such metals is considered vital to the industrial strategy of the UK as it moves towards Net Zero 2050 and the production of electric vehicles. www.cornishlithium.com. 

Published April 19, 2023

Topics: Mining

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more pr oductive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation supports sustainable lithium production