Remove a Redundant Module
To remove a redundant module, push the locking clips at the top and bottom of the module and slide the module out of the chassis.
IMPORTANT:
If you remove a redundancy module, you lose redundancy functionality.
If you want to resume system operation with an identical module, you must install the new module in the same slot.
Provide Feedback