Update Other Module Firmware in the Secondary Chassis

To update firmware for other modules in the secondary chassis, complete these steps.
  1. Optional: To replace module hardware, remove the module from the secondary chassis and replace it with the new module.
    Before you replace communication modules as part of this firmware update process, make sure that you first read Module Replacement. When replacing communication modules, the rotary switches and port configuration for the new modules must match the existing modules
  2. Launch
    ControlFLASH Plus®
    software.
  3. Update the firmware for modules other than the redundancy module.
  4. Close the
    ControlFLASH Plus®
    software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal