Set the Date and Time via Time Synchronization
You can use
CIP Sync™
time synchronization, also known as Precision Time Protocol (PTP), to sync the redundancy module date and time with a Grandmaster in the same chassis. The redundancy module can only receive time from the Grandmaster and cannot transmit time. Time synchronization is automatically enabled in the redundancy module and no further configuration is possible.To enable time synchronization on the redundant controller, see Enable Time Synchronization. For more information about
CIP Sync™
time synchronization in redundancy systems, see CIP Sync™
Time Synchronization.Provide Feedback