Assign a Chassis ID
To identify the physical chassis for a redundancy module as Chassis A or Chassis B, assign a chassis ID:
- If you change the chassis ID of the primary redundancy module, the secondary module is automatically assigned the other chassis ID.
- The chassis ID for a redundancy module becomes associated with its physical chassis, regardless of its primary or secondary control designation.
Chassis A is the default chassis ID.
Provide Feedback