Select Module Type dialog box overview
Use this dialog box to add devices to the
Logix Designer
application project. The Catalog
tab is the default tab of the Select Module Type
dialog box and presents a list of modules that is valid for the current context. Sort the Catalog Results list of modules based on Catalog Number
, Description
, Vendor
, or Category
. Use the Module Discovery
tab to perform online module discovery to find attached physical devices on a network or backplane. Use the Favorites
tab to customize the list of module types.To access the
Select Module Type
dialog box, from the Controller Organizer
,
right-click the I/O Configuration
folder and choose New Module
. The Select
Module Type
dialog box opens to the tab that was used most recently. Select the
Catalog
, Module Discovery
, or Favorites
tab to choose a module.You can also access this dialog box from the
File
menu, by choosing New Component
> Module
.Rockwell Automation recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback